Skip to Content
Skip over Language Selection
Skip over Primary Navigation
Skip over secondary navigation
Publishers Area
Skip over Contact, Sitemap
Skip over Search
[Advanced]
http://www2.sea.siemens.com | Multi-Enrollment Discounts | 2009-03-30
print
Siemens understands the importance of maximizing your training value. When enrolling a student into multiple courses such as S7 Programming 1-2-3 or enrolling multiple students into the same course, Siemens is pleased to offer the following Multi-Enrollment discount schedule.
Enrollments
Multiplier
Discount Percentage
2 - 5
0.90
10%
6+
0.85
15%
To qualify for the discount:
All enrollments in the cart must qualify or none will qualify.
All enrollments must occur within a 6 week window.
All enrollments must be booked on the same purchase order or credit card charge.
All students must be from the same company (the company name must be exactly the same).
Once booked, the total enrollment tuition, less the applicable discount will be invoiced at the start date of the first class.
Standard Payment terms apply. (See Standard Terms and Conditions.)
This discount cannot be combined with other discounts or promotional training programs.
Enrollments can be modified within the 6 week window and student names can be substituted freely. Late cancellation terms remain unchanged. (See Standard Terms and Conditions.)
Browse Course Schedules Now!
*This offer does not apply to Special Events, Online Classes, Excitation Systems, Process Analyzers, Process Instrumentation or Power Plant Control Solutions training.
Contact & Partner
Pre-sales info
Support
Training