Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

SE&A introduces Combination Type Arc Fault Circuit Interrupters

Electrical Fire

For Maximum Electrical Fire Safety Protection

The Residential Products Division recently announced the launch of a newly-enhanced version of the Siemens Combination Type Arc Fault Circuit Interrupter (AFCI) just one year after the first version of this product was introduced. 

This new compact AFCI device is equipped with Siemens patented unique LED trip indicators which will help electricians and home owners pinpoint the type of problems that cause the device to trip. The LEDs are located near the handle of the circuit breaker and will distinguish arcing faults, arcing to ground and over current conditions. The new Siemens Combination Type AFCI has been listed by Underwriters Laboratory Inc. and is available on 125-volt, single-phase 15 and 20 amp branch circuits in both plug in and bolt on versions.
Beginning January 1, 2008, the 2005 National Electrical Code (NEC) mandates the use of Combination Type AFCIs on circuits in bedroom areas in new residential construction. The 2008 NEC will expand the use of Combination Type AFCIs beyond bedrooms to protect all living areas.
Arcing faults are a major cause of electrical fires. Arcing can occur when a person hangs a picture and inadvertently pierces a wire in the wall or when old wires fray. The new Combination Type AFCI provides maximum electrical fire safety protection, because it protects against all three possible types of arc fault, line-to-ground, line-to-neutral arc, and series arcs. More info

Since the mid 90s, Siemens has invested in research and development and has partnered with industry innovators to develop arc detection technology. The Combination Type AFCI is a good example of how Siemens has used advanced technology to ensure fit, form and function for customers—technology that has been thoroughly tested by third-party laboratories and in the field. The device has the most compact size in the market place and includes the INSTA-WIRETM feature which saves electricians valuable time installing the device.

 

AFCI Circuit Breaker Technology from Siemens

 

New Troubleshooting Features

The new Combination Type AFCI provides unique LED trip  indicators that help electricians pinpoint the type of trip and save valuable time troubleshooting. For more information, please click here

 

AFCI Frequently Asked Questions

Got a question? Maybe our AFCI FAQ page can help you out.  Click here