Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

WHAT IS THE PURPOSE OF A CIRCUIT BREAKER?

The NEMA Circuit Breaker Section


Over the past half century, advances in molded case circuit breaker technology have led to a product that is a key element in the electrical safety of residences, office buildings, and sophisticated commercial and industrial systems. Circuit breakers have become so commonplace and reliable that their purpose is taken for granted and often misunderstood. In what ways do circuit breakers contribute to electrical safety? Under what conditions do they provide protection?

The National Electrical Code (NEC) defines a circuit breaker as follows:
A device designed to open and close a circuit by nonautomatic means and to open the circuit automatically on a predetermined overcurrent without damage to itself when properly applied within its rating.

Simply stated, a circuit breaker must be able to be switched open and closed manually and to protect a circuit from overcurrent by opening automatically. This allows a breaker to be used repeatedly without replacement.

The switching function of a circuit breaker is simple and readily understood. It provides a means of easily isolating a circuit or circuits protected by the circuit breaker from the rest of the electrical system, allowing for the safe modification or maintenance of the circuit, or equipment in the circuit. All circuit breakers are intended to switch loads. In addition, some are specifically rated for switching loads such as the lighting in commercial and in industrial buildings, on a regular basis.

The protection function is not quite so easily understood. What is a molded case circuit breaker intended to protect? What can an overcurrent protective device be expected to do and what is beyond the scope of its design? Sec. 240.1 (FPN) of the NEC has the following to say about overcurrent protection:
Overcurrent protection for conductors and equipment is provided to open the circuit if the current reaches a value that will cause an excessive or dangerous temperature in the conductors or conductor insulation.

So, circuit breakers are intended to protect conductors (insulated wires) by opening automatically before damage is caused by excessive temperatures. This protection applies to the permanently installed wiring of homes, offices, and industrial buildings. In protecting these wires, overcurrent protective devices reduce the risk of fire, personal injury, and damage to equipment and property.

Circuit breakers listed by UL are subjected to a rigorous test program to assure the specifications for overcurrent protection are met. Initial samples are subjected to endurance, overload and short-circuit tests with a length of the wire to be protected in the test circuit. Follow-up tests on samples randomly chosen from production samples are continually checked to be sure ongoing product is properly calibrated.

In summary, circuit breakers are intended to protect the wiring, permanently installed conductors and certain extension and power supply cords, from high temperatures caused by current in excess of the rating of the conductors. While "conductor" protection is the key element in electrical system safety, there are potentially dangerous conditions that do not involve overcurrent. Circuit breakers do not provide protection against these conditions. The following are important examples:

In summary, as defined by the NEC, circuit breakers provide switching and overcurrent protection functions. The overcurrent protection is a key element in electrical safety, protecting conductors from damage due to currents in excess of their ratings and reducing risk of fire, property damage, and personal injury. Special forms of circuit breakers can be applied to protect against damage due to ground fault and personal injury due to electrical shock.

However sophisticated and reliable, circuit breaker technology must be complemented by user and installer care and awareness if electrical safety is to be optimized.

Reprinted with permission from EC&M Magazine - copyright July 1994, Primedia Business Magazines & Media