Looking for Controlotron ? -- In 2006, Controlotron and Siemens signed an agreement whereby Siemens acquired the business activities of Controlotron. The New York based company is a leader in the development of the Clamp-On technology for ultrasonic flowmeters, which today is used in approx. 50% of all ultrasonic applications for fluids and gases.
Many of the former Controlotron product lines are still supported by Siemens Energy & Automation, Inc. The clamp-on ultrasonic flowmeter program consists of six product families, some targeting specific industries and some with general applicability over a wide range of different industries and applications.
SITRANS FUS1010 (Standard) and SITRANS FUP1010 (Portable)
General purpose liquid flowmeters. FUS1010 are dedicated wall mount units while FUP1010 are portable units that can be used for field surveys or temporary installations. Both are used for a wide variety of applications, including water & wastewater, HVAC, power and processing.
SITRANS FUE1010 (Energy)
These meters are ideally suited to thermal energy/power industry applications such as chilled & hot water sub-metering, condenser water, potable water and glycol and brine solution, thermal storage.
SITRANS FUH1010 (Oil)
These flowmeters are ideal for applications carrying crude oil, refined petroleum or liquefied gas. There are meters for two application areas: viscosity compensated volumetric flowmeters and standard volume (net) mass flowmeters.
SITRANS FUH1010
(Interface Detection) This interface detection meter is ideal for oil applications where a differentiation between various liquids in a pipeline is needed.
SITRANS FUG1010
(Gas)These gas flowmeters suit most natural and process gas applications, including checkmetering, allocation, flow survey verification, lost and unaccounted for (LAUF) gas analysis, production and storage.
SITRANS FUS1020
(Basic)These general purpose low cost flowmeters are suitable for many clean liquid applications in industries such as water & wastewater, chemical feed and HVAC and power.
Support:
Have questions about troubleshooting your products?
In the USA:
Customer Service:
Phone: 1-800-365-8766
E-mail: pibusales.sea@siemens.com
Technical Support:
Phone: 1-800-333-7421
E-mail: techsupport.sea@siemens.com
Repair
E-mail: pibusales.sea@siemens.com ATTN: RMA
To find local support worldwide search the Siemens global contact list. Links to technical documentation can also be found on the support page.
Need to Place an Order? Please contact your local sales representative. Sales locator In the USA
Global Sales locator.