PCS 7/APACS+ OS
A fully developed client framework provides the following key features:
Automatic rescaling to meet screen resolution needs
Alarm displays that show current alarms, current acknowledged alarms, alarms that have cleared but were not acknowledged, and operator action
A faceplate that can be called up directly from a specific alarm
Alarms that are automatically organized into areas
Security that can be easily implemented with users restricted to specific actions and areas
The integrated OS which combines the OS database, symbols and graphics, or pictures
Object symbols which are automatically placed on pictures and linked to objects in the controller; object symbols are automatically linked to faceplates
The banner display which is divided into control areas to provide graphic navigation and direct navigation in one mouse click to the graphic with an alarm
A built-in Report Designer which allows the user to schedule and run default, as well as user-created reports