Looking for the Answer
The vision for the future of Shell Chemical Company is to be the premier producer and preferred supplier of customer product needs. This includes being a world class performer in safety, health, environment, customer satisfaction and applied technology. Local management recognized this meant taking advantage of new technology, so we were encouraged to take risks along this line. With this support, we initiated a project to replace 1950’s vintage electrical equipment (switchgear, motor control centers, transformers, bus ducts, etc.) which provided electrical power to the plants utilitie infrastructure. Included in the project was a rudimentary PMCS. The first step was putting together a conceptual design team. The team consisted of electrical engineer discipline leader Billy Wright, Carl Reed, senior electrical inspector at the West Site, and Mark Plagens with Parsons, SIP, an Engineering, Procurement and Construction firm based in Houston.
We analyzed the plant's electrical system and determined its needs. To avoid possible equipment conflicts we decided to stay with a single supplier for the switchgear, motor control centers, and PMCS. A list of approved suppliers was developed and a preliminary evaluation was performed. The list was narrowed to Westinghouse Cuttler-Hammer, General Electric and Siemens Energy and Automation. In addition to the typical product literature, we received on-site presentations and, where available, visited other companies that had installed similar systems. We reviewed each from the standpoint of data collection, user friendliness, expandability and ability to interface with our existing components. We decided to stay with a Microsoft Windows based system with which our people were familiar. User friendly was a key issue for us. We wanted the system to be used and maintained, and that meant the people using it had to be able to learn it and keep it evergreen. We then developed location-specific Engineering Guidelines and Specifications which were included in the bid packages that were submitted to the three candidates.
Siemens was just introducing its WinPM software when we approached Gerry Thomas, Siemens industrial sales engineer based in nearby LaPlace. WinPM is an all-in-one, user friendly, menu-driven software that includes Dynamic Data Exchange to import and export data between itself and other software, and which uses standard Windows bit maps for graphics.
We liked the quality and availability of the equipment and parts as well as the company stability, the price offered, and the general direction Siemens was taking. They also impressed us with their enthusiasm, experience, and commitment, so the bid was awarded to Siemens. But now came the hard part*making it work for us and in a way that justified the change and outlay.
Blazing a Trail
We began working with the WinPM software at Norco in September 1994. As expected, the software was new and needed some bugs ironed out, so we were in regular phone contact with the Siemens people. We provided feedback and recommendations and they responded with product improvements. Visits to the Siemens factory provided opportunities for us to learn more about the program and again later, to test the software when the equipment was ready. After they installed the system, Siemens sent technicians to Norco and also troubleshot the system over the modem. One of our concerns had been that the manufacturer would continue to maintain and update its software; we gained assurances from Siemens when they committed to an additional 1.5 years of software support.
The motor installation proceeded on schedule but took a year to complete because it was being done hot. We had to swap over loads on tight time frames while making sure the old and new systems ran together smoothly. Out of 180 pieces of equipment switched, the only problem we had was one motor that ran in reverse and spun an impeller into a pump.
The System
For hardware, we located a computer with printer and monitor in a Retalle PC enclosure in one of the plant's substations and connected it via twisted pair wires to two switchgear units, each with 11 feeder breakers and six MCCs .
The computer is connected via fiber optic cable and modems to all the other substations in the site. Several isolated multi-drop RS232 to RS485 converters link different comm ports inside the console with Siemens Advanced Motor Master System (SAMMS), ACCESS I/O relays, 4720 meters and Static Trip III units in the switchgear and MCCs that make up the Siemens ACCESS PMCS.
The SAMMS units are solid state overload relays with integrated control logic designed to protect low and medium voltage motors. A sensor takes RMS current measurements and combines them with user-programmed full load amperes, service factor and trip class to prevent overload. Among other functions, they also protect motors from phase imbalance, load loss and ground fault.
The solid-state, addressable I/O relays allow remote control of contactors and breakers, while providing information on the status of field devices.
The 4720 power meters monitor the four incoming feeder lines as well as the medium and low voltage lines. These digital 4720s offer numerous metering functions, from min/max values and waveform capture to snapshot memory. They can also be used for a variety of control functions, such as load shedding and breaker tripping.
The Static Trip III devices are microprocessor controlled, RMS sensing over current protective relays with zone interlocking as a standard feature, for use in low-voltage switchgear. ISGS (Intelligent SwitchGear System) relays are provided for medium voltage applications, providing time delay trip and optional instantaneous trip for phase and ground elements.
By communicating with twenty-two 480V feeder breakers, eight MCCs and two enunciators that represent a total of 180 addressable devices, this one computer enables electrical personnel at the site to remotely program, monitor and control the electrical system within two substations.
A computer in another substation is running a separate system on WinPM, Impact, Excel and Multilin Relay Comm software that are tied together by the ACCESS system. This computer communicates with Siemens multi-drop converters which are looking at 4720s and ISGS relays inside that substation, as well as Westinghouse devices and Multilin meters and motor management relays.
The plan is to link both systems together over our LAN as soon as Siemens finalizes the networkability of its WinPM software. When that happens, the chemical facilities' electrical system will be accessible from any Shell facility in the country.