Realizing the Full Potential
Co-op members realized the potential the new system held. They began using the energy monitoring system to isolate peaks, and then worked backwards to the meters and then to the equipment that caused those peaks. They were then able to review options that would lead to reducing peak loads.
One example of end-user benefits is found at 77 W. Wacker Drive, a 50-story, Class Triple-A office tower in downtown Chicago and the headquarters of RR Donnelley & Sons. Tenants here expect to maintain a certain comfort level, especially during the summer. It was a challenge for us to find ways of reducing load while not inconveniencing the tenants. Eventually, we turned off some lights in the main lobby and shut off or cycled other equipment. For instance, we idled one elevator in each of the three banks.
To bring the tenants on board, we have used our quarterly newsletter to quantify the savings to them in kWh, and tied that in to our ongoing waste recycling program: "It's good for Chicago, it's good for the environment, and it helps us all." This message was reinforced by the ComEd rebate payments, which tangibly reduced truant occupancy costs.
When ComEd notified us about a scheduled curtailment, which might range in duration from two to the full six hour commitment, we made sure that the tenants were not adversely affected. We soon discovered the best approach was simply to lower the standard pressure on the fans to use less power. We also let hot water temperatures drop from 105 degrees to 90. We have never received a tenant complaint. In fact, the only way tenants might know that a curtailment is in progress is that the main lobby is slightly darker than usual.
The incentives for building management to participate in the curtailment program were energy conservation, goodwill with the tenants, and of course, the ComEd payments. But the greatest savings came from managing energy consumption by using the ACCESS system analysis capabilities. Each meter can be displayed and broken down on a spreadsheet against 30-minute demand, thereby enabling us to stay within or even to reduce ComEd's time-of-day/demand billing guidelines that determine customer rates.
As we became familiar with operating the system, we learned to connect it with the Building Automation System that controls the fans, chillers, the main power and mechanical equipment. The ACCESS system has the capability of compiling a memory of the building's operations, of knowing exactly when it can turn on a motor to meet set points while taking into account the demand factor.
Our long-term objective is to run the building with the most efficient use of energy possible. The Chicago real estate environment is highly competitive, so watching costs is a crucial management function. With automation, we've taken preemptive action to shave off those all-important usage peaks that the utility company uses to determine our rate of billing. We estimate that already we have lowered our electricity bills by 15% annually, and we project this reduction to eventually reach 30%.
Saving $100,000
Production facilities as well as office buildings have experienced appreciable benefits using the ComEd system. Just ask Dennis Cleary, Aseptic Supervisor at Chicago's McCain Citrus Inc., home of the BoKu brand of drinks. "Our main purpose in using this PC, over and above responding to ComEd's curtailments, is to manage our load and especially to control our demand," he says. "We have fluctuating demands from the four compressors we use to keep our 1 million cu. ft. freezer at 24 degrees below zero.
"During the summer, when the loading bay doors are left open, all four compressors kick in, and that creates a heavy demand. Fortunately, the PRMs can figure out demand instantaneously, so we set alarms for an instantaneous kW level before the fourth compressor kicks in. When the pop-up window comes on, we close the doors before we set a new peak.
"When we curtail, we shut down our 800 kW transformer in the engine room, which supplies all the compressors for the freezer. After five-to-six hours, the freezer rises from minus 24 to minus 14 degrees, so we are still within safety parameters.
"We also use the alarms on the system to monitor the unmanned engine room. If we have a failure, a pop up alarm appears on the screen. ComEd has certainly added value to the service they deliver with this system: I estimate we have saved $100,000 in electricity bills over the last three years, mainly as a result of utility payouts and reduced usage.
"The system has potential for further value. The long time pick-up data, for instance, will allow us to look into and fix overloads before they create outages and lost production."
Adding Still More Value
Some members still view the system as a glorified meter reader, not realizing the wide range of analysis tools available to them that can save them even more money.
Both ComEd and Siemens are working to educate end users on the different metering and hardware products, field gear, motor protection devices and other components that the ACCESS system comprises. The more users know about the system, the more they can do for themselves. They can, for instance, analyze and take steps to control power quality to avoid undervoltage conditions in one area without creating problems in another.
Users are now able to have sophisticated meters and relays with built-in power quality capability supplied on new electrical distribution equipment. They can also easily retrofit existing distribution systems with these same components. The difference between these kinds of devices and traditional "disturbance analyzers" are both technical and financial. While the capability of meters and relays used extensively on a day-to-day basis is not as great as what some might consider available from a fault recording device, the meters and relays have to be used in the power system anyway, for reasons involving protection and system design. Since these devices have to be present anyway, their additional capability for power quality data is essentially free.
Traditional fault recorders have been expensive portable devices, and must be moved to where a problem is believed to be, in hopes that it will be repetitive. Using meters and relays that will be in place all the time, faults and other power quality phenomena can be determined as soon as they occur, not after the fact. The data that is available from these devices includes both harmonic and transient information, and can be used by power system engineers to make recommendations which would minimize possible thermal damage from harmonics, or pinpoint the location and cause of dangerous faults, eliminating them in the future. From this data, engineers can make recommendations regarding the application of harmonic filters, or modified protection schemes to more reliably protect plant and personnel. Both harmonic and disturbance information will be used in the future to objectively rate power delivery by electrical distribution companies competing for end user business.
Customers who have their own transformers will be able to assess the exact load on each and then know whether they have enough capacity for expansion. At the moment, plants only know the total load of all transformers and so they typically add another one at great expense because they can't risk creating overloads.
Timely maintenance of equipment is a real system bonus: The power monitoring and control system can help determine which loads warrant maintenance (through its monitoring and recording of equipment usage) and therefore reduce downtime and maintenance costs. It allows proactive maintenance as opposed to a shotgun, gut-feeling approach to maintenance.
The system is invaluable for crisis management. It can isolate the cause of an outage immediately and help the building or plant return rapidly to normal operation. The appreciable benefits of the current system may soon be augmented by future developments. ComEd is taking the "EnergyTracker" concept further by designing a product that links its rates structure with data from meters so that customers can estimate their bills on-the-fly.