"When we weighed everything it just made sense to go with Siemens," Roe said. "The combination of PROFIBUS and AS-Interface bus interface work well together and give us intelligent MCC options."
PROFIBUS Reduces Installation, Start Up Times Roe said the decision to go with PROFIBUS for fieldbus communications immediately paid dividends. He said if the plant chose a standard, hardwired MCC lineup, eight wires would be needed to be connected to each of 194 motor starters -- going back and forth from the MCC to the control room 100 feet away.
"We had only two weeks to complete the entire MCC upgrade," Roe said. "We installed only four, ½" diameter PROFIBUS cables," Roe said. "If we hardwired, we would have had to pull 1,552 wires and drill through concrete to access that much conduit. Hardwiring would have taken seven electricians more than two weeks to finish 3,100 terminations. Also, hardwiring would have cost an additional $30,000 in labor and material costs if we had chosen conventional MCCs. We tore out the panelboards, put in the DCS, replaced all of the existing MCCs, removed all the wires and installed PROFIBUS, and tied it all back into the DCS in those two weeks."
John Richardson, automation specialist with Siemens Energy & Automation, said Arizona Chemical realized immediate and significant time and labor by using PROFIBUS during the check out and start up phases.
"Checking out the PROFIBUS communications was simply a matter of making sure the green indication light was on," Richardson said. "In fact, the Panama City plant technicians started the MCC twice, and went through the complete check out twice, because they didn't believe it could check out so fast."
Richardson also said Arizona Chemical saw the value in AS-Interface bus. He said the option of having power and communication over two wires further reduced wiring time and costs of the new MCCs. In addition, AS-Interface bus has enabled Roe and technicians at the plant to perform remote start/stop with just those two wires.
Enhanced Safety
Every time a problem arose with the old MCC line up, technicians were exposed to danger when buckets were replaced. The decades old MCCs were designed without protective barriers.
"The TIASTAR MCCs are fully insulated so that when the panels were opened, all of the bus was not staring right at you," Roe continued. "They have shutters so when electricians pull out a bucket out, the bus is not exposed, which was a major improvement."
Looking Ahead
Roe says a number of other upgrades have recently completed, are underway, or planned for the near future. A recent project involves not only Siemens control and distribution equipment, but advanced automation technology as well.
"We just installed SIMATIC S7300 PLCs on a waste water treatment system to help settle the solids, control the PH levels, and other functions," Roe said. "We used to have full time operators assigned to these areas. Now we are saving considerable costs by controlling these functions remotely."
The SIMATIC automation system controls multiple starters with a complicated pump sequencing operation, ensuring the pumps experience uniform wear.
"When we get a lot of rain water from hurricanes and other storms, we have to maintain proper levels or everything backs up into the plant," Roe said. "When all four of those 150 HP screw pumps are running, they can remove 30,000 gallons of water per minute.
"The TIASTAR smart MCCs, communications via PROFIBUS, and our experience with Siemens' automation technology have eliminated plant downtime and saved labor and material costs," Roe continued. "We now have more options to migrate to a more sophisticated DCS system, like Siemens PCS 7, when the time is right."