Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

Large AC Above NEMA Motors

Nema Motor

Large AC Motors Built to Meet the Most Demanding Standards

As one of the world’s leading providers of large motors with global service and support second to none, Siemens sells and manufactures a complete line of large AC squirrel-cage induction motors at its ISO-9001 Certified Norwood, Ohio, plant. This 350,000-square-foot facility has produced more than 150,000 high voltage motors continuously since 1898. The Norwood plant produces horizontal AC induction motors up to 10,000 horsepower and voltage ranges from 460 to 13,200 volts. The plant also manufactures a complete line of large AC vertical motors up to 6,000 horsepower.

For more than 100 years, Siemens large motors have earned a reputation for high performance, low maintenance and long service life in some of the world’s most demanding applications. It is this reputation, combined with unmatched service and support, that has made Siemens the leading supplier of motors around the world.

Siemens Meets or Exceeds Recognized Standards                                                                                               Siemens keeps its industry-leading reputation by staying at the forefront of important industry standards such as:

At Siemens, we listen to the needs of our customers and how they use motors. We then respond with motors that are designed and manufactured to provide maximum value for specific applications such as:

 
 

All About Large AC Above NEMA Motors