Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content
ControlNews

Headline Articles

Selecting Safety Networks – Why One Size Does Not Fit All
In safety networks, as in shoes, not only is it true that one size doesn’t fit all but it’s also the case that cost and performance matters. A shoe that’s right for a formal affair is likely to turn an ankle on a sports court. Likewise, a network suited for production or process level may not be the most efficient at the field level for example.

more

 

Announcements and General Product Information

KeySelectorSwitch.jpg

Announcing the Siemens Key Monitoring Selector Switch with Spring

How many times have you been in a plant where a key switch has the key in it? If you left the key in the switch, any employee could, at any time, put the safety relay in bypass creating production downtime. Every minute of downtime equals unearned revenue.   Reduce that downtown with Siemens Key Monitoring Selector Switches.

 

SIRIUS Detecting – The New Family of Position Switches

Our new comprehensive range of SIRIUS detecting devices is just what you need for nearly any field-level application. Our mechanical high-precision sensors dependably detect any motion sequence, convert the event into electrical signals and transmit the data to your control systems, so that you can immediately shut down your machines and systems if a fault occurs.

 

New Additions to the SIRIUS Line of Soft Starters

Our new 3RW40 is perfect for low HP loads with an economical and space saving package that is a family fit with our SIRIUS mechanical systems. The new compact 3RW40 offers soft start solutions that will save you space and overall cost with built-in bypass and overload protection as standard. Watch our website for the latest catalog.

 

The Exiderdome Traveling Expo brings experience and expertise to your doorstep

Join us as we unleash the imagination of Siemens with exiderdome, our innovative Industrial Automation Expo. This exciting hands-on environment gives you a unique opportunity to experience and find out more about the vital technologies that will transform the future of business.
In exiderdome, you’ll see amazing products, systems and solutions designed to help you boost productivity and reduce costs, today and tomorrow. Come to exiderdome and discover where state-of-the-art process and manufacturing automation and electrical infrastructure are headed. And unleash your own imagination.

 

Class 1 Div. 2 Approvals for SITOP Redundancy Module / SITOP Electronic Diagnostic Module

The Siemens Micro Automation Group is pleased to announce that the SITOP Redundancy Module and the SITOP Electronic Diagnostic Module are now approved for Class 1, Div.2 applications Group ABCD T4. This approval allows us to better meet the needs of the Oil and Gas Industry as well as meeting the requirements of certain applications in the Food and Beverage Industry.

 

New Addition to the SITOP Family of Power Supplies!

SITOP Modular 3-phase 24VDC/ 20A power supply, part number 6EP1436-3BA01 features a new compact design needs less than half the width and a three phase operation eliminates step-down-transformer!


Side Mounted Auxiliary Contact Kits for 30-400A CFS Switches

New catalog numbers CFS11AUX and CFS22AUX are in stock and are released for sale.   These new aux contact kits must be used when a CFSNFPA2 kit is used on a 30-400A CFS switch and auxiliary contacts are required.

 

TransCalc – Control Power Transformer Sizing Calculator – NOW ONLINE!

The NEMA & General Purpose Controls group is proud to introduce TransCalc. TransCalc is a control power transformer sizing calculator. In four easy steps, the user can determine the appropriate CPT size and catalog number as well as fuse sizes.

Not only can the user select from a list of standard products and modifications but as an alternative can directly enter the total inrush VA and sealed VA of the control circuit to be powered by the CPT.


Improved Assortment, Stock, and Lead-times for Pilot Devices!

At Siemens we know that four of the key factors in promoting Pilot Devices are Quality, Availability, Ease of Use, and a broad Product Line Assortment. The news for today is about changes that support the business side of our relationship with you.   That is, enhanced availability and assortment of our Pilot Devices. For more information, please see the attached form.

 

Knowledge Works NEMA Training – Now Open to Everyone!

Looking for a low-cost option to jump start your controls training? Siemens is pleased to announce our new on-line training courses focused on the basics of controls, starters and lighting contactors. And best of all it’s FREE! There is no cost to attend. You will receive a certificate upon completion of each module.


TD400C.JPG

New 4-Line Text Display Panel for S7-200

Released and available for ordering is the new TD 400C 4-line text display panel for the S7-200 micro PLC. The bright white-on-blue text panel can be configured for 4-lines of standard size text with up to 24 characters per line, or 2-lines of large size text allowing for maximum visibility.

Also included are 7 buttons for screen navigation and data entry, along with 8 user function buttons configurable for any desired equipment operation. All TD 400C control functions and display screens are developed using STEP 7 Micro/WIN PLC programming software for S7-200 micro PLCs, eliminating the need to maintain a separate PLC and HMI program.

The TD 400C supports customizable faceplates using the graphic overlay editor within STEP 7 Micro/WIN allowing customers to easily add company logos and button graphics to the front of their panel without any special ordering or custom manufacturing. The new TD 400C part number is 6AV66400AA000AX1 and is offered at a list price of $250ea.

 

New LOGO! USB Programming Cable

Released and available for ordering is the new LOGO! USB Programming Cable part number 6ED10571AA010BA0, list price $82ea. The new 1 meter programming cable allows users to connect their PC/PG through a USB port to any LOGO! controller for download/upload tasks using LOGO! Soft Comfort programming software. The new cable ships with a CD that includes USB driver support for Windows 98SE/XP/2000/Vista and Linux 2.6.