Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

AS-Interface Safety at Work

Safe and unsafe data on one bus system - AS-Interface Safety at Work makes it possible. Safety at Work utilizes the Actuator-Sensor Interface sensor level bus system as its foundation technology. AS-Interface is an OPEN protocol standard supported by hundreds of manufacturers worldwide. Connectivity to existing PLC platforms is possible by either using a standard AS-Interface Master in the central rack or by using protocol gateways, which connect many of the popular Fieldbus technologies to AS-Interface.

Standard AS-Interface slaves and Safety rated slaves can now co-exist on the same network. Systems that have an existing AS-Interface system can be easily expanded to use Safety at Work components. All that is required for a Safety at Work system is a Safety Monitor and Safety rated slaves. Safety rated slaves include E-Stop, position switches, light barriers etc. (up to EN954-1 category 4 are available). Up to 31 Safety rated slaves can be on one network. A maximum reaction time of the Safety Monitor is 40ms. Safety Monitors are available with either one or two output groups.

 
 

More Information on AS-Interface Safety at Work

More Information on AS-Interface Safety at Work

 
 

All About Automation

Siemens Automation MagazineBlogging @ SE&A