Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content
Image Guide Header Visual Product Page

Software Redundancy

Software redundancy – the cost-optimized solution

With the SIMATIC S7 software redundancy package, production-critical pro¬ces¬ses can be controlled on a fault-tolerant basis with the SIMATIC S7-300 and/or SIMATIC S7-400 standard automation systems for the very first time.

Thanks to this cost-effective software solution, production failures can be avoided when a fault occurs or when maintenance is being done. Many applications involve relatively slow processes which place few demands on the time needed for a switch-over in the event of a fault. The SIMATIC S7 software redundancy solution can therefore be used for the redundant control of pro¬ces¬ses for which a master-to-standby switch-over period in the seconds range is more than adequate.

Overview of further highlights:

 

All About Automation

Siemens Automation MagazineBlogging @ SE&A