Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

FAQ - Wireless

Q: What is Wireless Distribution System, WDS?

A: If a Wireless LAN needs to be upgraded, it is sometimes not possible to connect the access points over Ethernet to make communication beyond cells possible. Possible reasons:

In such situations, the access points can be used in the Wireless Distribution System mode without being wired.

In WDS mode, it is important that an access point can "see" its neighbors (otherwise the chain would be interrupted!). This can make it necessary to use special, distant antennas instead of the supplied antennas. As shown in Figure stations are perfectly capable of taking part in wireless operations in this mode. One important property emerges from its; namely, that stations and access points must share the entire data rate available. This situation can be made more critical because in WDS mode, ALL access points and stations work on the same wireless channel (for example 802.11g and channel 1, 2.4 GHz at 54 Mbps).

The performance of the wireless infrastructure in the above figure can be improved if dual access points (SCALANCE W788-2PRO) are used (see Figure 6). One wireless card can then be used to set up the wireless infrastructure (backbone) and the other wireless card provides the stations with a cell at the location of the dual access point with which they can access this wireless infrastructure. Once again, it is possible that special distant antennas may be required.

 
 

 
 

 
 

 
 

 
 

 
 

 
 

 
 

 
 

 
 

 
 

 
 

All About Scalance W (Wireless)

More information