Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

September 06, 2006

Introducing The New 1FT7 Synchronous Servomotor Series From Siemens

Chicago — At this year’s International Manufacturing Technology Show, Siemens Energy & Automation, Inc. will unveil the new 1FT7 series of synchronous servomotors for increased performance and user productivity.

This high-performance motor is up to 30 percent smaller than the 1FT6 series and offers users increased torque and a robust encoder attachment with convenient mounting options in a compact design.

The 1FT7 is the first servomotor with an encoder that can be replaced in the field without adjustment. Designed to withstand vibrations, the encoder operates without oscillations. Additionally, the encoder technology integrates with both SIMODRIVE and SINAMICS drives from Siemens.

Having been constructed with the flange on the drive end, the flat surface on the top provides expanded mounting options. A medium inertia motor designed for general machine tool applications, the 1FT7 series has a higher overload at 4 x MO (self-cooled) up to frame size 100. The flange on the drive end is also compatible with the 1FT6 series.

In addition to self-cooling, the new 1FT7 motors can be cooled through forced ventilation or water cooling through “COOL JETS” to lower the temperature of the motor. The cooling water connection, water flow and redirections are maintained exclusively in the end shield on the non-drive end. The 1FT7 series also has a higher degree of protection at IP64/IP65/IP67.“

The 1FT7 series was designed to meet the changing market needs with innovative new techniques,” said Rajas Sukthankar, marketing and business development manager. “With its convenient mounting, compact design and encoder technology, the 1FT7 is the new benchmark for servomotors.”

About Siemens

Siemens Energy & Automation, Inc. is one of Siemens' operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world`s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information: www.sea.siemens.com.

Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $96 billion in fiscal 2005. Founded nearly 160 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $18.8 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens` worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 460,000 people in 190 countries. For more information on Siemens in the United States: www.usa.siemens.com.