Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

January 23, 2008

New Guided Wave Radar Level Transmitters From Siemens

ATLANTA -- Siemens Energy & Automation, Inc. today introduced Sitrans LG200, a new line of guided wave radar level transmitters for liquids, slurries, interface, and bulk solids. Sitrans LG200 is a two-wire, loop-powered HART® level transmitter that can measure materials with a dielectric range of 1.4 and higher, temperatures up to 427 degrees Celsius (800 degrees Fahrenheit), and pressures up to 6250 psig (431 bar).

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
Alpharetta, GA 30005

michael.krampe@siemens.com

Related Photos