Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

October 17, 2006

Siemen Introduces A New Dimension In Monitoring Pumps

Houston — Siemens Energy & Automation, Inc. announced the introduction of a new acoustic diagnostics system for preventive maintenance on oscillating positive-displacement pumps. The Sitrans DA400 acoustic diagnostic system continuously monitors pump status and detects even the smallest leaks on pump valves.

The Sitrans DA400 is comprised of four acoustic sensors mounted on the pump and a diagnostics device connected to the sensor by up to 65 feet of cable. With continuous online monitoring, the ultrasonic acoustic sensors detect cavitation generated by the pump suction and discharge valves. The measurement results are displayed on the diagnostics device, or can be transferred to the control room over Profibus and analyzed in a control system like Simatic PCS 7. Any drop in pump efficiency is indicated, preventing unnecessary plant shutdowns.

The Sitrans DA400 system is suitable for all oscillating positive-displacement pumps used in mining, chemical/petrochemical industry and sewage treatment to pump fluids containing impure solids such as sludge. The diagnostics device is rated IP65 and can be operated between - 4°F and +140°F. The sensor is rated IP66/68 and operates between - 40°F and +230°F.

About Siemens

Siemens Energy & Automation, Inc. is one of Siemens' operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world`s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information: www.sea.siemens.com.

Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $96 billion in fiscal 2005. Founded nearly 160 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $18.8 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens` worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 460,000 people in 190 countries. For more information on Siemens in the United States: www.usa.siemens.com.

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-4959  
3333 Old Milton Parkway
Alpharetta, GA 30005

michael.krampe@siemens.com

Related Links: