Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

August 07, 2006

Newly Designed Landis & Gyr Line Of PAK Metering Now Available

ATLANTA — Landis & Gyr, a fully owned subsidiary of Siemens Energy & Automation, Inc. today announced the introduction of its new Landis & Gyr PAK metering equipment for utilities that require a lever bypass to service multiple meters in residential and commercial development projects. The unique lever bypass allows ease of maintenance and the utmost operator safety. Additionally, the PAK meter provides an all-in-one solution for applications needing from 2-6 meter positions, the new units feature a smaller, more compact design and lighter enclosures making it easier to install while using less wall space.

“Siemens is committed to developing innovative products that simplify power monitoring for our customers,” said Kevin Shumate, Product Marketing Manager. “The new line of PAK metering is a testament to this commitment, designed for safety, functionality, maximum flexibility and ease of installation.”

Installation of the new PAK metering is made faster and easier with the new Siemens exclusive angled circuit breaker mounting and floating deadfront, which eliminates the need for cover alignment of the breaker. Designed with the contractor in mind, the units feature side mounted handles that make it easier to lift and hanging brackets to suspend the unit during installation. The new units also have a mounting rail and generous wiring space.

Landis & Gyr will offer a full line of 2-6 position devices with provisions for one, two or three incoming conductors per phase and neutral. Additionally, an “In line” (column) construction is available for 2-4 and 5-6 position devices.

With 225 amp tenants breakers, the new PAK metering is 100K AIC rated. It meets the service requirements of multiple surface or semi-flush metering applications.

Additional features:

For more information about the new line of Landis & Gyr PAK metering, log onto www.sea.siemens.com/reselec/product/mfm.html.

About Siemens

Siemens Energy & Automation, Inc. is one of Siemens' operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world`s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information: www.sea.siemens.com.

Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $96 billion in fiscal 2005. Founded nearly 160 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $18.8 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens` worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 460,000 people in 190 countries. For more information on Siemens in the United States: www.usa.siemens.com.