Skip to Content


Skip over Language Selection

Change language to
  • English

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Contact, Sitemap

Contact, Sitemap

Skip over Search


Content

December 13, 2007

Award-Winning Combination Type ARC Fault Circuit Interrupter From Siemens is Now Available

Meets requirements of National Electrical Code® update effective Jan. 1, 2008

ATLANTA -- Siemens Energy & Automation, Inc. today announced that its full residential line of award-winning Combination Type Arc Fault Circuit Interrupters (AFCIs) is now available. Recently named “Equipment of the Year” by Independent Electrical Contractors (IEC), Siemens’ AFCIs meet all requirements of the current and proposed codes. The Combination Type AFCIs have been listed by Underwriters Laboratories Inc. (UL®) and are available for use on 120-volt, single-phase, 15- and 20-ampere branch circuits.

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
Alpharetta, GA 30005

michael.krampe@siemens.com